cancel
Showing results for 
Search instead for 
Did you mean: 

CMSIS V3.20 and CMSIS-RTOS V1.02

jim_wei
Associate II
Posted on January 19, 2014 at 07:38

I recently downloaded the latest STM32F4 Peripheral library, STM32F4xx_DSP_StdPeriph_Lib_V1.3.0.   The library contains peripheral driver and CMSIS V3.20 which includes CMSIS-RTOS V1.02.   In the CMSIS documentation that came with the download, there is a section talks about the using a CMSIS RTOS implementation.  The file structure of the following files are shown:

1. startup_<device>.s

2. system_<device>.c

3. <device>.h

4. <user>.c

5. cmsis_os.h

6. RTOS.LIB

7. RTOS_config.c

My question is, where are the RTOS.LIB and RTOS_config.c files?  I can not find them in the entire file strcuture of the library.  Has anyone used CMSIS-RTOS V1.02?

Thanks!

Jim

#latest-cmsis
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0