cancel
Showing results for 
Search instead for 
Did you mean: 

Change the Timer 2 to 32 bits

david.ye
Associate II
Posted on June 24, 2015 at 06:02

Hello,

I am using the timer 2 as a decoder of my motor wheel.

Problem is, the counting is going to fast and 16bits is not enough (4000 counting per revolution). I need more bits but the timer 2 has only 16bits, do you have any advice?

I've heard that it is possible to cascade the timer so it can count as one 32 bits, is that possible?

Thanks for the help
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0