cancel
Showing results for 
Search instead for 
Did you mean: 

Can you explain this code to me please ?

tamirmichael1975
Associate II
Posted on June 28, 2013 at 21:28

Hello,  Could somebody please explain why the code below (AN4099) does configure alternate function 2 for TIM2 (capture/compare channel 2) and yet configured channel 1 as well as an interrupt source? If it is desired to measure a signal low or high time, would you not expect one channel to be programmed as capturing both rising and falling edge? Thanks in advance!   void SIRC_Init(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

NVIC_InitTypeDef NVIC_InitStructure;

TIM_ICInitTypeDef TIM_ICInitStructure; /* Clock Configuration for TIMER */

RCC_APB1PeriphClockCmd(IR_TIM_CLK, ENABLE);

/* Enable Button GPIO clock */

RCC_AHBPeriphClockCmd(IR_GPIO_PORT_CLK, ENABLE); /* Pin configuration: input floating */

GPIO_InitStructure.GPIO_Pin = IR_GPIO_PIN;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(IR_GPIO_PORT, &GPIO_InitStructure); GPIO_PinAFConfig(IR_GPIO_PORT, IR_GPIO_SOURCE, GPIO_AF_2); /* Enable the TIM global Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = IR_TIM_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure); /* TIMER frequency input */

TIM_PrescalerConfig(IR_TIM, TIM_PRESCALER, TIM_PSCReloadMode_Immediate);

/* TIM configuration */

TIM_ICInitStructure.TIM_Channel = IR_TIM_Channel;

TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling;

TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

TIM_ICInitStructure.TIM_ICFilter = 0x0;

TIM_PWMIConfig(IR_TIM, &TIM_ICInitStructure);

/* Timer Clock */

TIMCLKValueKHz = TIM_GetCounterCLKValue()/1000;

/* Select the TIM Input Trigger: TI2FP2 */

TIM_SelectInputTrigger(IR_TIM, TIM_TS_TI2FP2);

/* Select the slave Mode: Reset Mode */

TIM_SelectSlaveMode(IR_TIM, TIM_SlaveMode_Reset);

/* Enable the Master/Slave Mode */

TIM_SelectMasterSlaveMode(IR_TIM, TIM_MasterSlaveMode_Enable);

/* Configures the TIM Update Request Interrupt source: counter overflow */

TIM_UpdateRequestConfig(IR_TIM, TIM_UpdateSource_Regular); IRTimeOut = TIMCLKValueKHz * SIRC_TIME_OUT_US/1000;

/* Set the TIM auto-reload register for each IR protocol */

IR_TIM->ARR = IRTimeOut; /* Clear update flag */

TIM_ClearFlag(IR_TIM, TIM_FLAG_Update);

/* Enable TIM Update Event Interrupt Request */

TIM_ITConfig(IR_TIM, TIM_IT_Update, ENABLE);

/* Enable the CC2/CC1 Interrupt Request */

TIM_ITConfig(IR_TIM, TIM_IT_CC2, ENABLE);

TIM_ITConfig(IR_TIM, TIM_IT_CC1, ENABLE);

/* Enable the timer */

TIM_Cmd(IR_TIM, ENABLE);  

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0