cancel
Showing results for 
Search instead for 
Did you mean: 

Can we use reserved location of IVT ? I want to use this to verify if I'm downloading correct hex file even though checksum is passed?

JSHAR.1890
Associate II

Can we use the reserved location of IVT as defined below 0x08000000

__vector_table
        DCD     sfe(CSTACK)
        DCD     Reset_Handler                     ; Reset Handler
 
        DCD     NMI_Handler                       ; NMI Handler
        DCD     HardFault_Handler                 ; Hard Fault Handler
        DCD     MemManage_Handler                 ; MPU Fault Handler
        DCD     BusFault_Handler                  ; Bus Fault Handler
        DCD     UsageFault_Handler                ; Usage Fault Handler
        DCD     0x08000000                        ; Reserved
        DCD     0                                 ; Reserved
        DCD     0                                 ; Reserved

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Yes. The CPU won't care about unused locations in the vector table as those interrupts should never get triggered.

If you feel a post has answered your question, please click "Accept as Solution".