cancel
Showing results for 
Search instead for 
Did you mean: 

Can we connect 2 camera with STM32N647A0

sakshi
Associate II

Hello everyone,

Can anyone guide/suggest, if we can connect 2 Camera of 8 MPx each with STM32N647A0.

Best Regards,

Sakshi 

1 REPLY 1
Ch_JE
ST Employee

Hello,

Yes, it is possible to connect two cameras to the STM32N647A0.

The STM32N647A0 supports dual camera inputs by using the DCMIPP as the main interface and optionally DCMI for a second camera.

Important Considerations:

Camera Resolution and Data Rate

Each 8 MP camera produces a high data throughput. You need to verify:

- Whether the DCMI & DCMIPP can handle the data rate.

- The available memory bandwidth to manage two video streams simultaneously.

- The camera modules’ interface compatibility (e.g., parallel DVP or MIPI CSI-2).

- If the STM32N647A0’s memory and processing resources meet your specific application requirements.

Additionally, review STM32Cube firmware application for DCMIPP to understand single camera integration, which can help as a baseline for dual camera setup.

Regards,