Question
CAN transmit status pending (STM32F105RB)
Posted on August 08, 2011 at 11:54
I wanted to run the CAN Interface of a STM32F105RB with the examplefile of ST (Can Network). The function CAN_TransmitStatus( CANx, 0x0) tells me that the status of transmission is pending. Do you have any idea's for this behaviour. I'm not able to send messages.
The PHY levels are 2.1 V for CAN-Low and CAN-High.