cancel
Showing results for 
Search instead for 
Did you mean: 

Can TIM1 be used for PWM input?

tamirmichael1975
Associate II
Posted on July 01, 2013 at 13:18

Hello,

Using STM32F407.

I need to measure the duty cycle of an external signal. I can use TIM4 + PWN input for that purpose, but it is merely a 16 bit counter (I need a 32 bit). I am using an Olimex STM32-E407 that only allows access to TIM2 (32 bit timer) via port E. But I cannot get the PWM input to work on it - which interrupt service routine should I use?

I see this in my header file

void TIM1_BRK_IRQHandler(void);       

void TIM1_UP_IRQHandler(void);        

void TIM1_TRG_COM_IRQHandler(void);   

void TIM1_CC_IRQHandler(void);        

not simply ''void TIM1_IRQHandler(void);''

So, if I can use PWN input for TIM1 (the reference manual says I can) which IRQ source do I need? Any information will be appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tamirmichael1975
Associate II
Posted on July 01, 2013 at 13:22

Please ignore the question above !