cancel
Showing results for 
Search instead for 
Did you mean: 

CAN normal mode

rajani
Associate
Posted on October 28, 2009 at 17:16

CAN normal mode

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
rajani
Associate
Posted on May 17, 2011 at 13:04

I have a problem in setting up CAN in normal mode. It is working well while in LoopBack, but not working when i change it to Normal mode.

My settings are given below..Please Let me know if anyone detect anything missing from this..

/* RCC setup */

RCC_DeInit();

/* Enable HSE */

RCC_HSEConfig(RCC_HSE_ON);

/* Wait till HSE is ready */

HSEStartUpStatus = RCC_WaitForHSEStartUp();

if(HSEStartUpStatus == SUCCESS)

{

/* HCLK = SYSCLK */

RCC_HCLKConfig(RCC_SYSCLK_Div1);

/* PCLK2 = HCLK */

RCC_PCLK2Config(RCC_HCLK_Div1);

/* PCLK1 = HCLK/2 */

RCC_PCLK1Config(RCC_HCLK_Div1);

/* Enable Prefetch Buffer */

FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

/* Select HSE as system clock source */

RCC_SYSCLKConfig(RCC_SYSCLKSource_HSE);

/* Wait till HSE is used as system clock source */

while(RCC_GetSYSCLKSource() != 0x04)

{

}

}

/* GPIOA and GPIOC clock enable */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_USART1 | RCC_APB2Periph_AFIO, ENABLE);

/* CAN Periph clock enable */

RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN, ENABLE);

/* GPIO setup */

GPIO_PinRemapConfig(GPIO_Remap1_CAN, ENABLE);// for remapping to PB8 & PB9

/* Configure CAN pin: RX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

GPIO_Init(GPIOB, &GPIO_InitStructure);

/* Configure CAN pin: TX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_Init(GPIOB, &GPIO_InitStructure);

/* NVIC interrupt setup*/

NVIC_InitStructure.NVIC_IRQChannel=USB_LP_CAN_RX0_IRQChannel;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

/* CAN setup and Transmit*/

// CAN register init

CAN_DeInit();

CAN_StructInit(&CAN_InitStructure);

// CAN filter init

CAN_FilterInitStructure.CAN_FilterNumber=1;

CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;

CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;

CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;

CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;

CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_FIFO0;

CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;

CAN_FilterInit(&CAN_FilterInitStructure);

// CAN cell init

CAN_InitStructure.CAN_TTCM=DISABLE;

CAN_InitStructure.CAN_ABOM=DISABLE;

CAN_InitStructure.CAN_AWUM=DISABLE;

CAN_InitStructure.CAN_NART=DISABLE;

CAN_InitStructure.CAN_RFLM=DISABLE;

CAN_InitStructure.CAN_TXFP=DISABLE;

CAN_InitStructure.CAN_Mode=CAN_Mode_Normal;//CAN_Mode_LoopBack;//

CAN_InitStructure.CAN_SJW=CAN_SJW_1tq;

CAN_InitStructure.CAN_BS1=CAN_BS1_8tq;

CAN_InitStructure.CAN_BS2=CAN_BS2_7tq;

CAN_InitStructure.CAN_Prescaler=2;// 8 MHz - (8/16)/250000

status=CAN_Init(&CAN_InitStructure);

if (status==CANINITOK)

{

/* CAN FIFO0 message pending interrupt enable */

CAN_ITConfig(CAN_IT_FMP0, ENABLE);

/* transmit 1 message */

TxMessage.StdId= 0x63A;

TxMessage.ExtId=0x200A;

TxMessage.IDE=CAN_ID_EXT;

TxMessage.RTR=CAN_RTR_DATA;

TxMessage.DLC=3;

TxMessage.Data[0]=0x00;

TxMessage.Data[1]=0xEE;

TxMessage.Data[2]=0x00;

ret=CAN_Transmit(&TxMessage);

}

/* CAN Receive */

void USB_LP_CAN_RX0_IRQHandler(void)

{

CanRxMsg RxMessage;

RxMessage.StdId=0x00;

RxMessage.ExtId=0x00;

RxMessage.IDE=0;

RxMessage.DLC=0;

RxMessage.FMI=0;

RxMessage.Data[0]=0x00;

RxMessage.Data[1]=0x00;

RxMessage.Data[2]=0x00;

CAN_Receive(CAN_FIFO0, &RxMessage);

}

jaripetteri
Associate
Posted on May 17, 2011 at 13:04

I have similar problem, did you manage to get your code work?