cancel
Showing results for 
Search instead for 
Did you mean: 

CAn frequency

Rizwan Syed
Associate II
Posted on April 18, 2017 at 12:39

Hi , 

How to calculate the frequency for CAN interface in 

STM32F769i-Eval board?

In CAN Example prescaler value is 4 and it is for 1MHz.

What should be the prescaler value for 250kb/s in source code?

Thanks and Regards

Rizwan Syed

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 18, 2017 at 14:10

Just do the maths, the CAN clock starts with the APB divides that down with the prescaler, and then divides again by the sum of the bit quanta settings.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..