BSP_AUDIO_OUT_Play function stops program execution
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-09-18 8:47 AM
Posted on September 18, 2016 at 17:47
Hi.
The function BSP_AUDIO_OUT_Play stops the program flow completely even before the return value can be read. The audio buffer is output as a never ending loop. The BSP_AUDIO_OUT_Init worked well with no error codes. I know now that my simple code should work since I've compared it to example codes. I've got the STM32F746G Discovery board and my project is at halt now since I need audio playback. Although the main program flow is stopped it seems I can flash a led from the SysTick callback routine. I've tried to trigger a BSP_AUDIO_OUT_Stop from the SysTick with no success. There must be a bug in any of the libraries that causes this behaviour and it is very serious. There is no way I can continue with my project until this problem is resolved. I have tried to tweak with many things and tried many clock configurations. No matter how slow I run the system clocks this problem persists. I've tried to run the function HAL_SAI_Transfer_DMA and that stops program flow too. Maybe this problem is related to DMA somehow. If anyone can provide a precompiled ''elf'' file of an example application so that I can verify that my board is ok would be greately appreciated. I cannot import example projects into System Workbench. Nor am I able to debug the code.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-09-21 9:11 AM
Posted on September 21, 2016 at 18:11
Hi,
We need more details about the issue you are facing : which firmware version using ? which BSP example are you based ? If possible to share your code.Regards