cancel
Showing results for 
Search instead for 
Did you mean: 

AN3374 In-application programming for STM3220G-EVAL Project size over 1K

sravanm
Associate
Posted on August 29, 2012 at 22:48

The binary_template project, (which is the project to be loaded via USART) compiles to be > 1K which is the limit for this project. Is there an updated version of this app note? I have all optimizations turned on and minimal scanf/printf for the library settings.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 29, 2012 at 23:13

The binary_template project, (which is the project to be loaded via USART) compiles to be > 1K which is the limit for this project. Is there an updated version of this app note? I have all optimizations turned on and minimal scanf/printf for the library settings.

 

What 1K limit? What tool chain?

Sector 0 accommodates 16KB of code. The Keil eval permits 32KB of code generation.

The application code portion has a limit of 1008 KB (ie 1 MB less the 16 KB the loader lives in), not 1000 bytes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sravanm
Associate
Posted on August 29, 2012 at 23:29

Ohh, 

okay well I misread that then, thanks for the quick reply!