cancel
Showing results for 
Search instead for 
Did you mean: 

AN3354 adaptation help?

bfeixas
Associate II
Posted on September 29, 2011 at 21:56

Hi,

I'm designing a program in order to read a USB stick using a USB Host, I've seen the example code given by ST with the appliaction note : AN3354. And I've bought the demo board necessary to prove the firmware but after looking carefully I've seen I haven't bought the right version of the demo board as it should be STM3210C-EVAL and my board it's STM3210C-SK/KEI, with some ports changed.

By now I haven't get to work this firmware.

So, any one could tell me which changes should I do in the firmware in order to work in my version of the demo board?

Thanks

#stm32f107-stm3210c
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0