cancel
Showing results for 
Search instead for 
Did you mean: 

afe4300 and stm32f103rb, rdy pin unchanged

DongJun Lee
Associate
Posted on May 23, 2017 at 12:04

Hello,

I have a problem in getting the ti AFE4300 start the ADC measurement. I started with a new board that was designed using reference design on TI. Am trying to communicate with the board through an stm32f103rb(nucleo).

I was set up spi mode 1 and want to use body composition measurement (BCM).

I give 1mHz to afe 4300 board by arm pwm signal.

These are what has happened

1. I can not read ADC data result register. when i read ADC data result, it just show only '0'.

2. the RDY pin status unchanged. it keep high status.

int main()

{

SystemInit();

UART2_Init();

DelayInit();

PWM_Init();

RESET_init();

init_spi1();

resetAFE4300();

initAFE4300();

initBCM();

//

while(1)

{

if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 1){

printf('register_Name\n\r');

printf('0x%X\n\r',readRegister(ADC_DATA_RESULT));

printf('0x%X\n\r',readRegister(ADC_CONTROL_REGISTER));

printf('0x%X\n\r',readRegister(MISC1_REGISTER));

printf('0x%X\n\r',readRegister(MISC2_REGISTER));

printf('0x%X\n\r',readRegister(DEVICE_CONTROL_1));

printf('0x%X\n\r',readRegister(ISW_MATRIX));

printf('0x%X\n\r',readRegister(VSW_MATRIX));

printf('0x%X\n\r',readRegister(IQ_MODE_ENABLE));

printf('0x%X\n\r',readRegister(WEIGHT_SCALE_CONTROL));

printf('0x%X\n\r',readRegister(BCM_DAC_FREQ));

printf('0x%X\n\r',readRegister(DEVICE_CONTROL_2));

printf('0x%X\n\r',readRegister(ADC_CONTROL_REGISTER_2));

printf('0x%X\n\r',readRegister(MISC3_REGISTER));

}

else if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 0){

//printf('%0x\n\r',readRegister(ADC_DATA_RESULT));

printf('low\n\r');

}

DelayMs(100);

}

}

void RESET_init(void){

GPIO_InitTypeDef GPIO_InitStructure;

//GPIO_PinRemapConfig(GPIO_Remap_SWJ_NoJTRST, ENABLE);

//GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);

/* Enable the GPIO Clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

/* Configure the GPIO pin */

GPIO_InitStructure.GPIO_Pin = PIN_RESET;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOC, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = SPI_CS_PIN;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = PIN_DRDY;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOC, &GPIO_InitStructure);

//

GPIO_SetBits(GPIOA, GPIO_Pin_4);

}

uint32_t RDY_read(void){

return GPIO_ReadInputDataBit(GPIOC,PIN_DRDY);

}

void RESET_HIGH(void){

//GPIOA->BSRR = PIN_RESET;

GPIO_SetBits(GPIOC,PIN_RESET);

}

void RESET_LOW(void){

//GPIOA->BRR = PIN_RESET;

GPIO_ResetBits(GPIOC,PIN_RESET);

}

void resetAFE4300(void){

RESET_LOW();

//printf('111');

DelayMs(100);

RESET_HIGH();

}

void init_spi1(void){ // for MASTER mode

GPIO_InitTypeDef GPIO_InitStructure;

SPI_InitTypeDef SPI_InitStructure;

// GPIO_StructInit (& GPIO_InitStructure);

// SPI_StructInit (& SPI_InitStructure);

/* Enable GPIOs clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

/* Enable SPI clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

/* Configure SPI SCK pin */

GPIO_InitStructure.GPIO_Pin = SPI_SCK_PIN | SPI_MOSI_PIN | SPI_MISO_PIN;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_InitStructure);

/* SPI configuration -------------------------------------------------------*/

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; //32

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

SPI_Init(SPI1, &SPI_InitStructure);

/* Enable SPI */

SPI_Cmd(SPI1, ENABLE);

}

void writeRegister(unsigned char address, unsigned int data){

unsigned char firstByte = (unsigned char)(data >> 8);

unsigned char secondByte = (unsigned char)data;

GPIO_ResetBits(GPIOA, GPIO_Pin_4);

SPI_SendByte(address);

SPI_SendByte(firstByte);

SPI_SendByte(secondByte);

GPIO_SetBits(GPIOA, GPIO_Pin_4);

}

int readRegister(unsigned char address){

int spiReceive = 0;

uint8_t spiReceiveFirst = 0;

uint8_t spiReceiveSecond = 0;

address = address & 0x1F; //Last 5 bits specify address

address = address | 0x20; //First 3 bits need to be 001 for read opcode

GPIO_ResetBits(GPIOA, GPIO_Pin_4);

SPI_SendByte(address);

spiReceiveFirst = SPI_SendByte(0x00);

spiReceiveSecond = SPI_SendByte(0x00);

GPIO_SetBits(GPIOA, GPIO_Pin_4);

spiReceive = (spiReceiveFirst << 8);

spiReceive |= spiReceiveSecond;

return spiReceive;

}

void initAFE4300(void)

{

writeRegister(ADC_CONTROL_REGISTER,0x5140);

writeRegister(MISC1_REGISTER,0x0000); //

writeRegister(MISC2_REGISTER,0xFFFF); //

writeRegister(DEVICE_CONTROL_1,0x0004); //Power down both signal chains

writeRegister(ISW_MATRIX,0x0000);

writeRegister(VSW_MATRIX,0x0000);

writeRegister(IQ_MODE_ENABLE,0x0000); //

writeRegister(WEIGHT_SCALE_CONTROL,0x0000);

writeRegister(BCM_DAC_FREQ,0x0040); //

writeRegister(DEVICE_CONTROL_2,0x0000);

writeRegister(ADC_CONTROL_REGISTER_2,0x0011);

writeRegister(MISC3_REGISTER,0x00C0);

}

void initBCM(void)

{

writeRegister(ADC_CONTROL_REGISTER,0x4120); //Differential measurement mode, 32 SPS //4120//C1A0

writeRegister(DEVICE_CONTROL_1,0x0006); //Power up BCM signal chain

writeRegister(ISW_MATRIX,0x0408); //Channels IOUTP1 and IOUTN0

writeRegister(VSW_MATRIX,0x0408); //Channels VSENSEP1 and VSENSEN0

writeRegister(ADC_CONTROL_REGISTER_2,0x0063); //ADC selects output of BCM-I output

writeRegister(WEIGHT_SCALE_CONTROL,0x0000); //Gain = 1 DAC Offset = 0 0x603F

writeRegister(BCM_DAC_FREQ,0x0032);

writeRegister(MISC3_REGISTER,0x0030);

}

uint8_t SPI_SendByte(uint8_t Data)

{

while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);

SPI_I2S_SendData(SPI1, Data);

while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);

return SPI_I2S_ReceiveData(SPI1);

}

Any leads would be of great help

Regards,

DJ

#afe4300 #stm32f103
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Diana Bogusz
Associate
Posted on January 10, 2018 at 21:23

I have exactly the same problem with afe4300 and stm32f100C8T6 microcontroller. Did you managed to solve this problem?

rohit
Associate

Can You send me your code and Schematic ,i will check

rohitpatil597@gmail.com

AIran
Associate

Hi, same problem here ... did anybody figure out what the problem is?