cancel
Showing results for 
Search instead for 
Did you mean: 

adding a button to the demo project

jasonedwards9
Associate
Posted on March 12, 2011 at 03:25

i managed to switch the LEDs around and add more LEDs to the demo code provided for hte ST32vldiscovery, but i would like some help understanding how the user button and the NISV interrupts work. What i want to do is add another button such that if i press it the program counts down - so the User button increases the LED flash rate and hte new button will decrease that rate.

the new button is added to port A bit 2

the changes i have made so far compile with the following warnings:

..\..\..\Utilities\STM32vldiscovery.h(122): warning:  &sharp47-D: incompatible redefinition of macro ''USER_BUTTON_PIN'' (declared at line 113)

..\..\..\Utilities\STM32vldiscovery.h(126): warning:  &sharp47-D: incompatible redefinition of macro ''USER_BUTTON_EXTI_PIN_SOURCE'' (declared at line 117)

..\..\..\Utilities\STM32vldiscovery.h(127): warning:  &sharp47-D: incompatible redefinition of macro ''USER_BUTTON_EXTI_LINE'' (declared at line 118)

..\..\..\Utilities\STM32vldiscovery.h(128): warning:  &sharp47-D: incompatible redefinition of macro ''USER_BUTTON_EXTI_IRQn'' (declared at line 119)

 

the changes i have made to the stm32vldiscovery.h file are as follows.

typedef enum

  BUTTON_USER = 0,

  BUTTON_USER1 = 1,   /*this is the new button name */

} Button_TypeDef;

/** @addtogroup STM32vldiscovery_LOW_LEVEL_BUTTON

  * @{

  */ 

&sharpdefine BUTTONn                          2     /* changed from 1 */

/* * @brief USER push-button

 */

&sharpdefine USER_BUTTON_PIN                   GPIO_Pin_0

&sharpdefine USER_BUTTON_GPIO_PORT             GPIOA

&sharpdefine USER_BUTTON_GPIO_CLK              RCC_APB2Periph_GPIOA

&sharpdefine USER_BUTTON_EXTI_PORT_SOURCE      GPIO_PortSourceGPIOA

&sharpdefine USER_BUTTON_EXTI_PIN_SOURCE       GPIO_PinSource0

&sharpdefine USER_BUTTON_EXTI_LINE             EXTI_Line0

&sharpdefine USER_BUTTON_EXTI_IRQn             EXTI0_IRQn

/* added by jase 5th March */

&sharpdefine USER_BUTTON_PIN                      GPIO_Pin_2

&sharpdefine USER_BUTTON_GPIO_PORT              GPIOA

&sharpdefine USER_BUTTON_GPIO_CLK              RCC_APB2Periph_GPIOA

&sharpdefine USER_BUTTON_EXTI_PORT_SOURCE      GPIO_PortSourceGPIOA

&sharpdefine USER_BUTTON_EXTI_PIN_SOURCE          GPIO_PinSource2

&sharpdefine USER_BUTTON_EXTI_LINE              EXTI_Line2

&sharpdefine USER_BUTTON_EXTI_IRQn              EXTI2_IRQn

from reading thru the code in the stm32vldiscovery.c file i dont think i need to add code to the pin configuration part because it takes in the definitions from the h file.

any help would be much appreciated 

#external-interrupts-button
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 12, 2011 at 04:57

You're second set of #define's basically reassign the first set, because they have the same names, but with different content/assignments.

You need something like

#define USER_BUTTON0_PIN                   GPIO_Pin_0

#define USER_BUTTON1_PIN                   GPIO_Pin_2

#define USER_BUTTONx_PIN ...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..