2014-02-17 8:43 AM
Hello
Can any one help me how to configure the ADC of the stm32f3 in the injected trigered mode.(TIM1 CC4 trigger).2014-02-17 9:06 AM
Review how it's done on the F1, adapt
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\ADC\TIMTrigger_AutoInjection\main.c2014-02-17 10:58 PM
I tried to do that, but still I have a problem in starting the ADC injected conversion:
the ADC Init function: /* Enable ADC1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); /* ADC Channel configuration */ /* GPIOC Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div4); /* Configure ADC Channel7 as analog input */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); ADC_StructInit(&ADC_InitStructure); /* Calibration procedure */ ADC_VoltageRegulatorCmd(ADC1, ENABLE); /* Insert delay equal to 10 µs */ Delay(10); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1) != RESET ); calibration_value = ADC_GetCalibrationValue(ADC1); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Clock = ADC_Clock_SynClkModeDiv4; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0; ADC_CommonInit(ADC1, &ADC_CommonInitStructure); ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable; ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); /* ADC1 regular channel7 configuration */ ADC_InjectedChannelConfig(ADC1, ADC_Channel_7, 1, ADC_SampleTime_1Cycles5); ADC_ExternalTriggerInjectedConfig(ADC1,ADC_ExternalTrigInjecConvEvent_1,ADC_ExternalTrigInjecEventEdge_RisingEdge); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* wait for ADRDY */ while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY)); /* Start ADC1 Software Conversion */ ADC_StartConversion(ADC1); ADC_ITConfig(ADC1,ADC_IT_JEOC,ENABLE); NVIC_InitStructure.NVIC_IRQChannel=ADC1_2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority=1; NVIC_InitStructure.NVIC_IRQChannelCmd=ENABLE; NVIC_Init(&NVIC_InitStructure);2014-02-18 4:56 AM
2014-02-24 12:31 AM