cancel
Showing results for 
Search instead for 
Did you mean: 

ADC + DMA (8Channels) Aleatory Crash

gui2
Associate II
Posted on March 17, 2015 at 13:23

Hello,

I've an application that need the reading of 8 ADC channels...

I had thought use DMA in order to collect a big amount of data and then calc the average.

Everything works great! However, sometimes, in an aleatory way, the code crashes! :(

Any suspicion?

Here is my configuration:

#define NSAMPLES    35

#define NUM_CHANNELS    8

#define DMA_BUFFER_SIZE (NSAMPLES*NUM_CHANNELS)

void ADC_Configuration(void)

{

  ADC_InitTypeDef       ADC_InitStructure;

  ADC_CommonInitTypeDef ADC_CommonInitStructure;

  DMA_InitTypeDef       DMA_InitStructure;

 

  /* Enable peripheral clocks *************************************************/

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); NO init params

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

 

  /* DMA2_Stream0 channel0 configuration **************************************/

  DMA_DeInit(DMA2_Stream0);

  DMA_InitStructure.DMA_Channel = DMA_Channel_0;

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(ADC1->DR);

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ADC1_Buff;

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

  DMA_InitStructure.DMA_BufferSize = DMA_BUFFER_SIZE;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;

  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init(DMA2_Stream0, &DMA_InitStructure);

  /* DMA2_Stream0 enable */

  DMA_Cmd(DMA2_Stream0, ENABLE);

  

  /* Configure ADC1 Channels pins as analog input ******************************/

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_2  |  GPIO_Pin_3 |  GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 ;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  

 

  /* ADC Common Init **********************************************************/

ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

ADC_CommonInit(&ADC_CommonInitStructure);

 

/* ADC1 Init ****************************************************************/

ADC_Cmd(ADC1, DISABLE);

ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

ADC_InitStructure.ADC_ScanConvMode = ENABLE;

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStructure.ADC_NbrOfConversion = NUM_CHANNELS;

ADC_InitStructure.ADC_ExternalTrigConv = 0x00;

ADC_Init(ADC1, &ADC_InitStructure);

  

/* Enable ADC1 DMA */

ADC_DMACmd(ADC1, ENABLE);

ADC_RegularChannelConfig(ADC1, ADC_Channel_3 , 1, ADC_SampleTime_480Cycles);  

ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_480Cycles);  

ADC_RegularChannelConfig(ADC1, ADC_Channel_2 , 3, ADC_SampleTime_480Cycles); 

ADC_RegularChannelConfig(ADC1, ADC_Channel_6 , 4, ADC_SampleTime_480Cycles); 

ADC_RegularChannelConfig(ADC1, ADC_Channel_5 , 5, ADC_SampleTime_480Cycles); 

ADC_RegularChannelConfig(ADC1, ADC_Channel_4 , 6, ADC_SampleTime_480Cycles);  

ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 7, ADC_SampleTime_480Cycles); 

ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 8, ADC_SampleTime_480Cycles);  

    

  /* Enable DMA request after last transfer (Single-ADC mode) */

  ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);

  

  ADC_ContinuousModeCmd(ADC1, ENABLE);

    /* Enable ADC1 **************************************************************/

  ADC_Cmd(ADC1, ENABLE);

 

    Delay_ms(100);

    /* Start ADC1 Software Conversion */

    ADC_SoftwareStartConv(ADC1);

}

Thanks in advance!

Best regards,

--

Guilherme

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 17, 2015 at 16:33

Everything works great! However, sometimes, in an aleatory way, the code crashes! :(

 

Any suspicion?

Random crashes, probably not this code. Check you have adequate stack, and try to provide more information on what a ''crash'' means in this context. Where does the processor go if you stop execution? Is it in the Hard Fault handler?

You'll need to get a lot more specific on what happens to understand why it happens.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..