Using STM32F429I-Discovery as USB OTG MSC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-25 9:29 AM
Hi
My company wants to evaluate the STM32F429I-Discovery kit and its functions.One of the applications I have to develop will consist in using the board itself as a USB OTG Mass Storage Class, so that I can transfer files and data from my PC to its internal memory.I did the job, using the examples provided by the STM32F4Cube. I work with the Keil MDK-ARM.ST-Link V2 driver installed and working fine. I can program and debug the card.But my problem is that when connecting the board to my PC (Windows 8 installed), it is not recognized.In the Device Manager it appears as a ''unknown device'' with error ''Windows has stopped this device because it has reported problems. (Code 43)''.In the properties the events say:Device USB\VID_0000&PID_0002\6&7e58c76&0&1 had a problem starting.But I had filled the device description structure with:__ALIGN_BEGIN uint8_t USBD_HS_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END = { 0x12, /*bLength */ 0x01, /*bDescriptorType*/ 0x00, /*bcdUSB */ 0x02, 0x00, /*bDeviceClass*/ 0x00, /*bDeviceSubClass*/ 0x00, /*bDeviceProtocol*/ 0x40, /*bMaxPacketSize*/ 0x83, /*idVendor*/ 0x04, /*idVendor*/ 0x2A, /*idVendor*/ 0x57, /*idVendor*/ 0x00, /*bcdDevice rel. 2.00*/ 0x02, 0x01, /*Index of manufacturer string*/ 0x02, /*Index of product string*/ 0x03, /*Index of serial number string*/ 0x01 /*bNumConfigurations*/ } ; I tried to reconfigure the GPIO (pin, pull, mode...) ,timers,, etc... now my PC sees the board as a ''USB Mass Storage device'' but produces the following status:''This device cannot start. (Code 10)''and event details:Device USB\VID_0483&PID_572A\00000000001A had a problem starting.Driver Name: usbstor.infClass GUID: {36FC9E60-C465-11CF-8056-444553540000}Service: USBSTORLower Filters: Upper Filters: Problem: 0xAStatus: 0x0So I can't find exactly what I have to program and configure.Which GPIO should I use and which configuration ?What about the system clock ? Should I use the RCC HSE ?What about the NVIC ?How do I configure the SDRAM ?As you see I am quite lost. I tried to use the STM32CubeMX but this does not help a lot.Has someone already worked on this type of project ?Is it really possible to use the STM32F429I-Discovery itself as a USB OTG MSC ?If I could have technical tips and even some examples, that would be great.Thanks in advance for your help #stm32f4-usb #msc- Labels:
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-01 10:23 AM
int8_t STORAGE_Write (uint8_t lun,
uint8_t *buf,
uint32_t blk_addr,
uint16_t blk_len)
{
memcpy((void *)(0xD0000000 + (0x200 * blk_addr)), buf, (0x200 * blk_len));
return(whatever);
}
int8_t STORAGE_Read (uint8_t lun,
uint8_t *buf,
uint32_t blk_addr,
uint16_t blk_len)
{
memcpy(buf, (void *)(0xD0000000 + (0x200 * blk_addr)), (0x200 * blk_len));
return(whatever);
}
Probably no examples, cause it's trivial. In reality you'd want to range check the inputs, and return success or failure codes as required. Look at what template you have now.
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
‎2014-08-06 10:00 AM
Well, I had already done something similar but I can't go further.
Whe I try to access it from my Windows Explorer, I receive continuous interruptions in:void HAL_PCD_IRQHandler(PCD_HandleTypeDef *hpcd)In this function there is a test to see if the USB is in device mode: /* ensure that we are in device mode */ if (USB_GetMode(hpcd->Instance) == USB_OTG_MODE_DEVICE) ...Function is coded as:uint32_t USB_GetMode(USB_OTG_GlobalTypeDef *USBx){ return ((USBx->GINTSTS ) & 0x1);} When debugging I see that hpcd->Instance = 0x0 and this GINTSTS is set to 0x080004DDSo USB_GetMode() returns 1 instead of 0But I have configured USB as OTG device in my usb_conf.c.I did this using examples from the STM32CubeF4 and STM specifications.So I have a doubt concerning my config.For using the Discovery board as a USB device Mass Storage, do you know what is exactly the configuration to use ?Which GPIO do I have to use and with which config ?Here is what I have:void HAL_PCD_MspInit(PCD_HandleTypeDef* hpcd){ GPIO_InitTypeDef GPIO_InitStruct; if(hpcd->Instance==USB_OTG_FS) { /**USB_OTG_FS GPIO Configuration PA9 ------> USB_OTG_FS_VBUS PA11 ------> USB_OTG_FS_DM PA12 ------> USB_OTG_FS_DP */ GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; /*GPIO_SPEED_LOW*/ GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Peripheral clock enable */ /* Enable USB FS Clocks */ __USB_OTG_FS_CLK_ENABLE(); /* Peripheral interrupt init*/ /* Sets the priority grouping field */ HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4); HAL_NVIC_SetPriority(OTG_FS_IRQn, 7, 0); HAL_NVIC_EnableIRQ(OTG_FS_IRQn); } else if(hpcd->Instance==USB_OTG_HS) { /* Peripheral clock enable */ __USB_OTG_HS_CLK_ENABLE(); /**USB_OTG_HS GPIO Configuration PB12 ------> USB_OTG_HS_ID PB13 ------> USB_OTG_HS_VBUS PB14 ------> USB_OTG_HS_DM PB15 ------> USB_OTG_HS_DP */ GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_14|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* Peripheral interrupt init*/ /* Sets the priority grouping field */ HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4); HAL_NVIC_SetPriority(OTG_HS_IRQn, 7, 0); HAL_NVIC_EnableIRQ(OTG_HS_IRQn); }}USBD_StatusTypeDef USBD_LL_Init (USBD_HandleTypeDef *pdev){ /* Init USB_IP */ if (pdev->id == DEVICE_FS) { /* Link The driver to the stack */ hpcd_USB_OTG_FS.pData = pdev; pdev->pData = &hpcd_USB_OTG_FS; hpcd_USB_OTG_FS.Instance = USB_OTG_FS; hpcd_USB_OTG_FS.Init.dev_endpoints = 7; hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL; hpcd_USB_OTG_FS.Init.dma_enable = DISABLE; hpcd_USB_OTG_FS.Init.ep0_mps = DEP0CTL_MPS_64; hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED; hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE; hpcd_USB_OTG_FS.Init.low_power_enable = ENABLE; hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE; hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_FS.Init.use_external_vbus = ENABLE; HAL_PCD_Init(&hpcd_USB_OTG_FS); HAL_PCD_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_FS, 0, 0x40); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_FS, 1, 0x80); } if (pdev->id == DEVICE_HS) { /* Link The driver to the stack */ hpcd_USB_OTG_HS.pData = pdev; pdev->pData = &hpcd_USB_OTG_HS; hpcd_USB_OTG_HS.Instance = USB_OTG_HS; hpcd_USB_OTG_HS.Init.dev_endpoints = 11; hpcd_USB_OTG_HS.Init.speed = PCD_SPEED_FULL; hpcd_USB_OTG_HS.Init.dma_enable = ENABLE; hpcd_USB_OTG_HS.Init.ep0_mps = DEP0CTL_MPS_64; hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_EMBEDDED_PHY; hpcd_USB_OTG_HS.Init.Sof_enable = DISABLE; hpcd_USB_OTG_HS.Init.low_power_enable = ENABLE; hpcd_USB_OTG_HS.Init.vbus_sensing_enable = DISABLE; hpcd_USB_OTG_HS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_HS.Init.use_external_vbus = DISABLE; HAL_PCD_Init(&hpcd_USB_OTG_HS); HAL_PCD_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x174); } return USBD_OK;}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-06 11:33 AM
Attached is the .HEX file from a quick port of my STM32F4-DISCO-SDIO-MSC to STM32F429I-DISCO-SDRAM-MSC, I used the original USB Firmware library (I don't use/support HAL/CUBE) and built it with GNU/GCC (Yagarto 4.7.2)
Updated with a build that retains SDRAM content as long as board is powered. ________________ Attachments : stm32f429i_discovery_msc_sdram_001.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0ZY&d=%2Fa%2F0X0000000bak%2FJu1jXvNAK_cQunC4R_dApQW6g4rV.c8fZCXnQltP.iA&asPdf=falseUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-12 7:38 AM
All right, finally I got it. When looking at your hex file, I found that I had a bad serial number.
As I have coded my application to support both FS and HS USB, the real values should have been:#define USBD_MSC_SERIALNUMBER_STRING_HS ''000000000001A''#define USBD_MSC_SERIALNUMBER_STRING_FS ''000000000001B''Now it works. I can write and read data to the device connected in MSC mode.But my problems are not over :)I have another application for testing the USB in CDC mode. It works.But now I would like to have one single application to support both MSC AND CDC.But I have a problem with the descriptors.Which values should be set ?Is 000000000001A/000000000001B pair correct for a USB composite ?I think no, but I don''t know which values should be used.Do I have to keep the same PID for both MSC and CDC descriptors ?In stm32f4xx_it.c I have to handle interrupts. So I coded this:void OTG_FS_IRQHandler(void){ HAL_NVIC_ClearPendingIRQ(OTG_FS_IRQn); HAL_PCD_IRQHandler(&hpcd_USB_OTG_MSC_FS); HAL_PCD_IRQHandler(&hpcd_USB_OTG_CDC_FS);}void OTG_HS_IRQHandler(void){ HAL_NVIC_ClearPendingIRQ(OTG_HS_IRQn); HAL_PCD_IRQHandler(&hpcd_USB_OTG_MSC_HS); HAL_PCD_IRQHandler(&hpcd_USB_OTG_CDC_HS);}Do you think this is correct ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-17 12:04 PM
Hello michel.j
Just curious if you got it working and if you can share your code. Thanks, Valentin
- « Previous
-
- 1
- 2
- Next »