cancel
Showing results for 
Search instead for 
Did you mean: 

usb msc file copy stall

dragan
Associate II
Posted on February 04, 2012 at 18:49

usb msc file copy stall

#usb-msc #usb #stm32f2xx #stm32f2xx-us
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dragan
Associate II
Posted on February 14, 2012 at 18:47

Body of my original post didn't make into the discussion board.

Has anybody noticed the following issue:

I noticed that copy from the MSC device to PC will stall if:

 uint8_t array MSC_BOT_Data[MSC_MEDIA_PACKET]

is allocated at address 0x125A4 or higher.

This array is used as a data buffer for DMA handling transfer.

Workaround: When I allocated MSC_BOT_Data to addresses bellow 0x125A4 (by moving my application code to the bottom group in the Keil project file) the problem goes away.