cancel
Showing results for 
Search instead for 
Did you mean: 

USB FS Device question

hpipon957
Associate III
Posted on January 16, 2012 at 13:38

Hi All

I am wondering about the USB FS device defines below:

typedef union _USB_OTG_DIEPINTn_TypeDef

{

  uint32_t d32;

  struct

  {

uint32_t xfercompl :

    1;

uint32_t epdisabled :

    1;

uint32_t ahberr :

    1;

uint32_t timeout :

    1;

uint32_t intktxfemp :

    1;

uint32_t intknepmis :

    1;

uint32_t inepnakeff :

    1;

uint32_t emptyintr :

    1;

uint32_t txfifoundrn :

    1;

uint32_t Reserved08_31 :

    23;

  }

  b;

} USB_OTG_DIEPINTn_TypeDef ;

Checking the data sheets for the various parts I don't see any emptyintr or txfifoundrn bits (also no ahberr  bit). These positions are all marked as reserved.

Reserved08_31 should be Reserved09_31 but this is not important.

Checking some example ST code, the txfifoundrn bit is in fact set during the USB device initialisation. Is this of importance??

Regards

Mark

#usb
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0