cancel
Showing results for 
Search instead for 
Did you mean: 

[Synopsys OTG] FIFO clash

waclawek.jan
Super User

So where exactly does the documentation say that different FIFOs can't be accessed simultaneously?

In dervice mode, an In endpoint was configured to transmit one 16-byte-long packet, and then 16 bytes (i.e. 4 words, 72 43 70 A4 D9 99 55 2E 19 7F 32 37 13 EB B6 7E) were being written to the endpoint's Tx FIFO, in "main" (and instrumentation and logging confirmed they were indeed written to the FIFO all, as 4 words), when the USB interrupt kicked in and it read from the Rx FIFO. The result on the bus was:

0690X000006C5xoQAC.png

So what we see here? The USB core decided to transmit the first 5 bytes, 72 43 70 A4 D9, and appended the CRC calculated from the first 4 bytes of these 5. Naturally, host refused to ACK this. Core retried 2 more times, and the apparently gave up, inserting a zero-length DATA0 packet at 475 607 517ns (not expanded on that view, sorry). Then the USB core skipped 3 bytes (I'd say, in the first case it took 2 words, but used only one byte of the second word) and then transmitted one byte, with the CRC of 0 bytes (i.e. 0000). Rinse and repeat. Then core threw transfer complete interrupt and everything proceeded as usually.

I've seen similar patterns with the data packet containing 13 bytes, with CRC of the first 12 of them.

Preventing the USB interrupt to kick in solved the problem entirely; and also helped selectively disabling the particular interrupt resulting in reading from Rx FIFO (and not running any other In endpoint i.e. writing to some other Tx FIFO).

The "factory" firmware fills FIFOs only in the interrupt so it won't be hit by this. This is nice, but IMO working more by accident than by deliberate design, given the documentation doesn't appear to talk about conflicting FIFO accesses. In fact, there's nothing which would indicate, that the individual endpoints are not completely independent from each other.

I don't say this wasn't fun to find, but I am supposed to work and not having fun the whole day.

JW

20 REPLIES 20

> Is your original finding that FIFO operations can clash or is it only that interleaving OTG register access between partial FIFO writes can clash?

I don't know.

It's been quite some time, and these days I don't have the resources to dig deeper.

JW