cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7s78-DK , TCP/IP +LWIP+freeRTOS

HarshthaR
Associate II

Hi

I have implemented TCP/IP with LWIP, but after enabling the freeRTOS, I'm facing lot of issues, ping is not happening, flash overflow errors , internal flash is very less need to use external flash(how to configure?). 
Mainly I need to enable freeRTOS to existing TCP/IP program . Along with that linker file which one to use as please let me know. .rodata overflow, something I getting error.

I've attached the project for reference.

Please give reply at the earliest.

Thanks,

Harshitha R

0 REPLIES 0