STM32F4DISCOVERY USB Audio Device works but ...
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-03-11 11:22 PM
Posted on March 12, 2013 at 07:22
I have got the USB Audio Device example working on the stm32f4discovery board . When connected to my laptop via usb , the board can be recognized as an speaker. There is audio output from the headphone when play music on my laptop .However , the audio output is really funny , women sounds like man in the output of the board .
It seems that the I2S output clock frequency of the dicovery board is slightly higher than the audio sample rate of the laptop output . Is there a way to make the I2S output clock frequency the same with the audio sample rate of the laptop output? ----------------------------------- I have changed the I2S input clock from 3840000 to 86000000 by generating another system_stm32f4xx.c file.It is much better now , still not perfect. #stm32f4discovery-usb-audio
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-03-05 12:23 AM
Posted on March 05, 2014 at 09:23
I have the STMF4 Discovery working as USB Audio Sound Card.
Project and few details are here: www.tjaekel.com Best regards Torsten