Skip to main content
MauFanGilaMedical
Associate III
May 14, 2025 8:52 AM UTC
Question

Processor stuck if I run code without debugger

Hello.

I have developed an application with touchgfx, lwip, freertos.

I had some problems with lwip (see processor goes to HardFault at __ISB - STMicroelectronics Community, HardFault_Handler when enable LWIP and touchgfx - STMicroelectronics Community).

I understand some causes of HardFault and this morning code seems to work properly.

 

I tried to run the code without debugger but my processor stuck in some point that I can't see because I have no debugger connected.

 

I reconnect debugger, reflash and rerun. After this operations I obtain the problem described in processor goes to HardFault at __ISB - STMicroelectronics Community

 

Why processor run with debugger but it stucks without it ?

 

Thankyou in advance.

 

 

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
May 14, 2025 9:09 AM UTC

@MauFanGilaMedical wrote:

I tried to run the code without debugger but my processor stuck in some point that I can't see because I have no debugger connected.


Add instrumentation so that you can see where it's hanging; eg,

  • UART output;
  • LEDs; 
  • Pins observable on scope/logic analyser;
  • etc, ...

LwIP debug output: https://community.st.com/t5/stm32-mcus/using-the-itm-console-for-printf-redirects-and-lwip-debug/ta-p/723472 

 


@MauFanGilaMedical wrote:

Why processor run with debugger but it stucks without it ?


Suggests a timing issue:

  • Debugger adds some start-up delays - so code works;
  • Without debugger, no delays, so something(s) is/are not ready - so doesn't work.

See: https://community.st.com/t5/stm32-mcus-embedded-software/basic-udp-echo-server-works-in-debug-but-not-run-mode-nucleo/m-p/787083/highlight/true#M61552 

 

#Instrumentation #CodeInstrumentation #DebugVisibility

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MauFanGilaMedical
Associate III
May 14, 2025 9:24 AM UTC

yes, you are right... I'm doing now..thankyou

Andrew Neil
Super User
May 14, 2025 1:31 PM UTC

@MauFanGilaMedical wrote:

I tried to run the code without debugger but my processor stuck in some point that I can't see because I have no debugger connected.


Note that you can attach the debugger to an already-running system - so you can see where it is "stuck":

Disable the Reset:

AndrewNeil_1-1747229331738.png

Disable the download:

AndrewNeil_2-1747229387268.png

and you don't want it doing a build:

AndrewNeil_3-1747229428452.png

 

 

#ConnectToRunningTarget #ConnectToCrashedTarget #ConnectToHungTarget

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
May 15, 2025 8:22 AM UTC

@MauFanGilaMedical  - I think you're a bit premature in marking my post as the solution: that post just contains some suggestions for how  to debug the issue - it's not actually a solution to the problem.

See this for how to un-mark a solution.

 

Take a look at the two posts by @Guillaume K in this thread:

https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/778561

do they address your issue?

In particular, are you getting the mentioned ERR_RTE error?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MauFanGilaMedical
Associate III
May 21, 2025 12:46 PM UTC

No, I don't have RTE error, I commented SCB_InvalidateDCache_by_Addr because it is exceuted even if I have disabled DCache.

 

Now it works