cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in Simultaneous Record and Play

ngupta7373
Associate
Posted on September 11, 2015 at 18:30

Hi,

  I'm trying to write an application to do simultaneous record and play on the STM32F4Discovery board. (16 KHz, 2 Channel, 16-bits). The audio quality on the speaker is not good in this case.

  Thereafter, I tried to do this sequentially instead of simultaneously. I first record into a 40960 bytes buffer and then play from that buffer. The sequence is:

BSP_AUDIO_IN_Init()

BSP_AUDIO_IN_Record()

// Record Samples

BSP_AUDIO_IN_Stop()

BSP_AUDIO_OUT_Init()

BSP_AUDIO_OUT_Play()

// Play the same buffer

BSP_AUDIO_OUT_Stop()

  This sequence runs correctly for the first time and I'm able to hear the recorded audio correctly. But when I run this in a loop for the second time, the audio is highly distorted. I can barely make out what was spoken during recording.

  Could you please advise on anything that I might be doing wrong.

thanks,

Ngupta

#stm32f4discovery-audio
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0