Open port error on host while using HAL_Delay
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-19 3:03 AM
I use STM32F407G-DISC1 board. I have run some examples with VCP based on STD library. Everything is OK. Then I have tried to generate code by CubeMX. And something interesting happens.
If not to add any code, then VCP is defined by host and Terminal can connect that.
If I add CDC_Transmit_FS in endless loop of main(), it works
volatile uint32_t time_var = 3e7;
while (1){
while(time_var) {
time_var--;}
CDC_Transmit_FS(b, 4);
time_var = 3e8;}
If instead of internal while loop I use HAL_Delay function, then terminal can't open the port.
while (1) {
Hal_Delay(5e3);
CDC_Transmit_FS(b, 4);}
So, COM port is defined in DeviceManager, but terminal can't connect that. It happens even before the first call of CDC_Transmit_FS, though hUsbDeviceFS is already initialized. The following code runs OK again.
while (1) {
Hal_Delay(5e3);
//CDC_Transmit_FS(b, 4);}
I have tried to increase Heap size, it doesn't help.
#open-port-error #cdc #vcp
- Labels:
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-27 3:29 AM
Same problem, still no any solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-27 5:44 AM
Hello,
This should be related to interrupts priorities: check USB and SysTick priorities.
As you may have already noted it in any readme file of the Cube examples, we have following recommendation:
'Care must be taken when using HAL_Delay(), this function provides accurate delay (in milliseconds) based on variable incremented in HAL time base ISR. This implies that if HAL_Delay() is called from a peripheral ISR process, then the HAL time base interrupt must have higher priority (numerically lower) than the peripheral interrupt. Otherwise the caller ISR process will be blocked.To change the HAL time base interrupt priority you have to use HAL_NVIC_SetPriority() function.'
-Amel-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-27 5:59 AM
On the other hand...
If I use CUBE MX generated project for the GCC, without any source code modification -- project works fine time-to-time. But if I will place simple source code part on the main function -- project does not working always (Open port error on host)
for (unsigned char i = 0; i < 32; i++)
{ transmitBuffer[i] = i + 1;}P.S.
I was trying to play with 'heap_size', 'V_bus'... Results is sameSTM32f4-Discovery
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-10 10:06 AM
Actually the problem is not in using delay function. If I add some other code, then the problem is the same 'open error port'.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-10 10:12 AM
Somethere in configuration there is an error. I have made the following thing.
1. Create project as described here
http://visualgdb.com/tutorials/arm/stm32/usb/
2. Copy all files relating to usb (drivers, config...) in my environment.
3. It works with the last hal drivers, and clock settings generated by cube.