cancel
Showing results for 
Search instead for 
Did you mean: 

Need technical support in getting the USB HID power Device driver or code which can be ported to STM32F401.

BSing.0
Associate

Hi , We designed a USB host dongle board using STM32F401 MCU. And want to read the data from a APC power device through USB port. We are able to detect Keybaord device through that but look like to read the data from APC power device we need to add the USB power device sub class. Do you have any application or off the shelf driver or code for the USB power device. Which can be ported to STM32 to make it work with APC power device?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0