Jump in memory issue in C on STM32L152
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-07-03 1:08 AM
Posted on July 03, 2015 at 10:08
Hello everyone,
I made a custom bootloader for my stm32L1 but my problem resides in jumping at the beginning of the flash when my new binary file is loaded.I made some research on this subject.. the PC and the MSP register need to be changed with the new address.Here is the function I made to jump in memory but it doesn't work and I don't understand why..t_error Jump_to_app(pFunction Jump_To_Application, uint32_t JumpAddress) {if (((*(__IO uint32_t*) WRITE_START_ADDR) & 0x2FFE0000) == 0x20000000) { JumpAddress = *(__IO uint32_t*) 0x08000004; Jump_To_Application = (pFunction) JumpAddress; __set_MSP_BOOT(*(__IO uint32_t*) 0x08000000); Jump_To_Application(); } else { return (NOK);} return (OK);This function doesn't work but when I press the RESET button, the jump works and my binary is executed.. but I can't figure why this function doesn't do the magic..I checked on the Eclipse debugger the value of the MSP register seems to be good : 00400120 Maybe the PC register is not modified.. I really have no ideas If someone knows a way to made simples jump in memory using C, it would be very helpfull !!! #stm32 #bootloader #c #jump
Labels:
- Labels:
-
Bootloader
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0