cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Emulation read write crashes program STM32L412

MikeLemon
Associate II

Hello, 

I try to write some user parameters to the non volatile memory of the program like using an EEProm , trying to read or wrote to say memory address 0x08019000 keeps crashing my program and debugger when reading / writing from it.

I see from the memory scan with the debugger that address  0x08019000 did infact get written by luck in one of my many attemps today but still can't read / write to it realy.

Here are the base functions I use:

```

uint32_t flashWriteData(uint32_t Address, uint64_t data){

  HAL_FLASH_Unlock();
  FLASH_EraseInitTypeDef EraseInitStruct;
  EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
  // EraseInitStruct.Banks = FLASH_BANK_1; // ?
  EraseInitStruct.Page = Address;
  // EraseInitStruct.NbPages = 1;

  uint32_t PageError;
  if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)    //Erase the Page Before a Write Operation
      return HAL_ERROR;

  // HAL_Delay(50);
  HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,Address,(uint64_t)data); // FLASH_TYPEPROGRAM_DOUBLEWORD FLASH_TYPEPROGRAM_WORD
  HAL_Delay(50);
  HAL_FLASH_Lock();


}


uint32_t flashReadData(uint32_t Address){

  __IO uint32_t read_data = *(__IO uint32_t *)Address;
  return (uint32_t)read_data;
}
```
 
Useage:
 
```

  uint32_t *MyData;

  MyData = flashReadData(0x08019000);

  printf("My Data = %d\n", *MyData);

  if(MyData == 55){
    printf("Variable has already been written to\n");
  }
  else{
    printf("Was %llu Now Writing to variable\n", MyData);
    uint64_t MyWriteData = 55;
    flashWriteData(0x08019000, MyWriteData);

  }
 
  uint32_t *MyReadData = flashReadData(0x08019000);

  printf("My Read Data = %d\n", *MyReadData);
 
```
 
 
Any idea what am I doing wrong

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Mkotb
Associate II

@MikeLemon  Did you find away for this, as I'm facing the same issue ?

liaifat85
Senior III

You can try this way.

uint32_t MyData;
MyData = flashReadData(0x08019000);

printf("My Data = %lu\n", MyData);

if (MyData == 55) {
    printf("Variable has already been written to\n");
} else {
    printf("Was %lu. Now Writing to variable\n", MyData);
    uint64_t MyWriteData = 55;
    flashWriteData(0x08019000, MyWriteData);
}

MyData = flashReadData(0x08019000);

printf("My Read Data = %lu\n", MyData);
Mkotb
Associate II

@liaifat85 and what about flashWriteData and flashReadData, are they the same as up or what ?