Skip to main content
IKhan.2
Associate
May 18, 2021
Question

I/O pin internal short to VCC

  • May 18, 2021
  • 2 replies
  • 1191 views

Can desoldering and soldering to replace a capacitor which is part of an RC filter of an I/O pin cause that pin to develop an internal short to VCC?

 

This problem has now happened on 14 PCBAs. Any insight would be gratly appreciated.

 

Regards

ik

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 18, 2021

Let's say it would surprise me, more likely solder reflow or esd.

Perhaps protect the chip more during the process, and be very quick. Use an ESD safe soldering station, and make sure that's working properly.

Look at the solder mask, and how much the board house shrunk that back, and what other things are in the proximity of the part changed, and that the capacitor part itself is not defective.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
May 18, 2021

I have done this many many times and never developed an internal short to ground on a pin. I would look into your process and how the rework is being done.

"If you feel a post has answered your question, please click ""Accept as Solution""."