2020-04-22 3:00 AM
In 'X-CUBE-NFC6', I found the prefix code of NFCID2 in SENSF_RES is '0x02, 0xFE'. But the ISO 18092 says:
The 6-byte number shall be randomly generated while the prefix code is ‘01’ ‘FE’. Other settings for the prefix code are RFU.
So, what's the meaning of '0x02, 0xFE' here?
Solved! Go to Solution.
2020-04-22 6:19 AM
Hi,
please refer to NFC Forum Digital protocol:
Table 46: NFCID2 Format
Byte 1 Byte 2 Byte 3 – Byte 8 Description
01h FEh Dynamically Generated NFC-DEP Protocol supported
02h FEh Device Identification Type 3 Tag Platform supported
All other values Proprietary Identification Type 3 Tag Platform supportedISO18092 describes P2P based on NFC-DEP. So obviously they use 01 FE.
The X-CUBE-NFC6 example emulates an NFC Forum T3T (card specimen: FeliCa Lite-S).
Regards, Ulysses
2020-04-22 6:19 AM
Hi,
please refer to NFC Forum Digital protocol:
Table 46: NFCID2 Format
Byte 1 Byte 2 Byte 3 – Byte 8 Description
01h FEh Dynamically Generated NFC-DEP Protocol supported
02h FEh Device Identification Type 3 Tag Platform supported
All other values Proprietary Identification Type 3 Tag Platform supportedISO18092 describes P2P based on NFC-DEP. So obviously they use 01 FE.
The X-CUBE-NFC6 example emulates an NFC Forum T3T (card specimen: FeliCa Lite-S).
Regards, Ulysses