cancel
Showing results for 
Search instead for 
Did you mean: 

VDD and VDD_TX connection in X-NUCLEO-NFC06A1 circuit schematic

DSai.1
Associate III

Dear Sir,

In st25r3916 datasheet, VDD and VDD_TX is not connected togather.

But in X-NUCLEO-NFC06A1 circuit schematic, it seems that these two

pins are connected togather, but there is a X sign in schematic as shown

in attached figure.

could you like to confirm this connection for us?

VDD and VDD_TX should be connected or not for normal application?

best regards

Dai Sai

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi Dai Sai,

not sure about the meaning of the X. But the chapter about "Power supply system" clearly tells "VDD and VDD_TX must be connected to the same power supply."

Best Regards, Ulysses

View solution in original post

2 REPLIES 2
Ulysses HERNIOSUS
ST Employee

Hi Dai Sai,

not sure about the meaning of the X. But the chapter about "Power supply system" clearly tells "VDD and VDD_TX must be connected to the same power supply."

Best Regards, Ulysses

DSai.1
Associate III

Dear Ulysses,

thank you very much for your reply.

I misread the figure 2 in datasheet of st25r3916.

It is good to confirm that VDD and VDD_TX is connected in our PCB.

best regards

Dai Sai​