2018-10-16 6:27 AM
Hey there ,
I have just revived ST25R3911B disco board. For the testing purpose I'm using ST25-pc and GUI app. I can get the UID for the ISO14443A and ISO15693 , but my ultimate goal is to read and write the selected sector of Mifare 1K along with the authentication key, but i haven't found any SW packages for the same
Can you please help me to develop the SW package
Thanks
Solved! Go to Solution.
2018-10-17 12:42 AM
Hey,
please see https://community.st.com/s/question/0D50X00009XkgK1SAJ/st25r3911b-and-mifare-classic-supporting
Regards, Ulysses
2018-10-17 12:42 AM
Hey,
please see https://community.st.com/s/question/0D50X00009XkgK1SAJ/st25r3911b-and-mifare-classic-supporting
Regards, Ulysses
2018-10-17 12:57 AM
Hey thanks Ulysses for the feedback
but why you're not providing crypto1 cipher based firmware?
As i have ordered the official Disco board of STM and I'm expecting the support from the community
i really Don't know why ST25 needs external Crypto 1 cipher ? I have already use PN 532 with arduino that doesn't required Crypto 1
Thanks
2018-10-17 2:53 AM
is it possible to read and write mifare 1k without Crypto-1 ?
2018-10-17 7:47 AM
Hi Mahendra,
to my best knowledge Mifare Classic (1K,4K) can only be read/written after successful authentication (crypto1).
PN532 has a built-in crypto1.
Regards, Ulysses
2018-10-17 11:43 PM
Hey thanks for your feedback
Yes, have go through the datasheet of the PN532 and PN7150 that i have used earlier and also read the datasheet of ST25R3911B
mostly NXP's reader ic have built in Crypto -1 engine as they are the proprietor of the Crypto-1. unfortunately the algorithm was buggy and easy to hack, even Mifare 1K getting clone by the little efforts and that's why NXP have clarify about the Antilogarithm an it's security, later
But Right now I'm seeking for the Support from STM to get the Crypto-1 software packages ind-order to write and read the Mifare 1K with authentication
Here is the Macros that contains the code for the same in ST25R3911B software packages
#include "mcc.h"
#include "mcc_raw_request.h"
#define HAS_MCC
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.