2019-08-20 1:25 AM
Hi
I am using the NFC5 V1.3.0 for the STM32L053R8-Nucleo as an example to port the RFAL library for using with either a STM32F051 or STM32G071.
I replaced the Systick/NVIC/EXTI/GPIO/SPI Hal and everything seems to work, except that when I want to read out the UID of the used tag NFCV-15693 only 5 Bytes are read from the FIFO. On the Nucleo-Board the detection works fine.
Do you have any idea where my problem is?
Attached is the SPI communication with the not working MCU.
Thanks in advance.
Best regards
Patrick
Solved! Go to Solution.
2019-08-20 2:20 AM
I fixed the problem which was related to the SysTick Timer.
Best regards,
Patrick
2019-08-20 2:20 AM
I fixed the problem which was related to the SysTick Timer.
Best regards,
Patrick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.