cancel
Showing results for 
Search instead for 
Did you mean: 

NFC antenna - total resistance of antenna copper traces

JPehl.1
Associate III

According to this values on eDesign Suite:

0693W000001pKRrQAM.png

What would be the resistance of the entire trace, from one edge to other, in ohms? NXP calculator gave result as 2,05 ohms on their tool. But I am here to ask what would be the actual resistance of the antenna above? I need to know the resistance to calculate the EMI filter and coupling components.

Can I rely on that 2,05 ohms value?

Regards.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Henry Crane
ST Employee

Hello,

a simulation of your antenna leads to 2 ohms for the real part of impedance at 13.56MHz.

By experience, this result shall be multiplied by 1.5 or 2 to fit with measurements done using network analyzer or impedance analyzer.

best regards,

Feel free to contact us for more information,

Henry Crane NFC/RFID support.

View solution in original post

2 REPLIES 2
JPehl.1
Associate III

I have used some online copper trace resistance calculators and had result of around 1.6~1.65 ohms.

parameters are:

  • thickness = 1/2oz = 18um
  • width = 0.25mm
  • length = 418mm

I got that 1.6ohm result on 5 calculators, so it should be correct. And I will use that value on the ST25R95 filter and matching calculation.

I just need to know the correct value to input it on the spreadsheet.

Current layout of NFC is on right: 0693W000001pKpZQAU.png

Henry Crane
ST Employee

Hello,

a simulation of your antenna leads to 2 ohms for the real part of impedance at 13.56MHz.

By experience, this result shall be multiplied by 1.5 or 2 to fit with measurements done using network analyzer or impedance analyzer.

best regards,

Feel free to contact us for more information,

Henry Crane NFC/RFID support.