cancel
Showing results for 
Search instead for 
Did you mean: 

Adafruit ST25DV16K not able to write a link that has more than 24 characters using HelloWorld

ETann.1
Associate

I'm having a bit of trouble with my Adafruit st25dv16 and the HelloWorld library.

Specifically, I'm running into a problem when I try to write links that are longer than 24 characters.

I've noticed that I can write shorter links and read them just fine using my mobile device. However, whenever I try to read a link that's longer than 24 characters, I get a "null" message instead.

I was wondering if you might be able to offer some advice on how I can work around this issue. Do you know if it's possible to write longer links to the Adafruit st25dv16 using the HelloWorld library? Or maybe there are some other libraries or tools I could use instead?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Schuyler
Senior

是�?�有代�?�?编写和读�?�?

Translation:

"What is the difference between the two?"

parata.carlo
ST Employee

Hello @ETann.1​ ,

what is your hardware setup? Which HelloWorld library are you using? Please, could you provide more information about your hardware and software setup?

Best Regards,

Carlo