cancel
Showing results for 
Search instead for 
Did you mean: 

VIPerPlus: Smart Off-line Converters

difranco.fabrizio
Associate II
Posted on February 12, 2010 at 09:59

The release to market of the VIPer25,26 (available soon),27, and 28 of the VIPerPlus family of Off Line High Voltage converters complements the previously released VIPer15,16,17 devices.

ST Advantages:

 

  • 800V HV Mosfet with integrated current sense and thermal sensing
  • Low standby power consumption to meet industry standards
  • Current mode control for simple loop compensation
  • Over current, over voltage and thermal protection with auto restartcapability
  • No Aux winding required for VIPer26 application
  • VIPer28 can deliver higher peak power
  •  Selectable frequency range

e-Presentations:

http://www.st.com/stonline/domains/support/epresentations/viperplus/viperplus.htm

More info:

http://www.st.com/viper

 

#viperplus
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
zracrusa
Associate
Posted on May 11, 2010 at 00:19

Fabrizio,

I am working a circuit using VIPER53E parts, and I need some technical help in getting the breadboard going. My application is to develop this power supply at 300KHz (see attached Viper file), but evertime I put the input DC voltage to about 120V, the front end blows and I burn up the Viper53 chip. I need some help in understanding this chip's operation and what I am doing wrong in the breadboard stage.

Got to go, please email me with an idea or some technical material on how the Viper53E chip works. I need this ASAP.

regards,

dave albert

011-506-293-3468 (Costa Rica, Central America)

________________

Attachments :

viper53-e.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htzo&d=%2Fa%2F0X0000000ab9%2FDqWeMk5osAJ0W80l5BTWKwxKVnz8nDbTgsIs6Ij86o8&asPdf=false
mallik.ranajay
Associate II
Posted on May 18, 2010 at 09:43

Hi Dave,

Just to understand:

When you mean breadboarding an SMPS, do you have a proper PCB? I am assuming you do or it will not work

Second, try putting a 60/100W domestic incandescent light bulb in series with the input. This will limit the current and you will not blow off the Viper53 easily. If something is wrong, the bulb will keep on glowing brilliantly even at no o/p load and you can quickly switch off the input supply!

 And ramp up the input 120 Volts using a variac or something while monitoring the drain voltage w/form just after the UVLO threshold has crossed. Do not apply it in full. You should see oscillations starting.

Are the transfomer  winding phasing maintained as it should be for a flyback?

Best regards.

Ranajay