cancel
Showing results for 
Search instead for 
Did you mean: 

STM32100B-MCKIT with MotorControl-Library STM32 PMSM FOC Firmware Library v3.0 web distribution

foelling
Associate
Posted on May 09, 2012 at 16:42

Hello everyone,

I am working on the Motor Control Kit consisting of:

- STM100B-EVAL Evaluation Board with STM32F100VB (Medium Density, Value Line)

- STEVAL-IMH023V2 Motor Control Demonstration Board

I am porting the MC Projects (MC Application - RELEASE and UserProject - STM32100B-EVAL) from IAR Embedded Workbench IDE to KEIL IDE.

 

I am nearly finished, at least I have one problem:

According to the readme.txt

- STM32100B-EVAL: to configure the project for STM32 Medium-density Value

 

line devices

 

@note The needed define symbols for this config are already declared in the

 

preprocessor section: USE_STDPERIPH_DRIVER, STM32F10X_MD_VL, USE_STM32100B_EVAL

 

my Compiler / Preprocessor Defines are:

USE_STDPERIPH_DRIVER,

STM32F10X_MD_VL,

USE_STM32100B_EVAL

In main.c (Line 49) I get Error ''

Invalid configuration: MCU definition in Control stage parameters.h not compatible with selected board

'' because STM32PERFORMANCE is defined.

Background: main.c includes Parameters conversion.h, that includes Control stage parameters.h. Here, im Line 27 STM32PERFORMANCEMD is defined witout any condition.

/* STM32PERFORMANCEMD or STM32VALUELD or STM32VALUEMD or STM32PERFORMANCEHD */

 

#define STM32PERFORMANCEMD

This leads in Parameters conversion.h in Line 788 to:

#if (defined STM32PERFORMANCEMD) || (defined STM32PERFORMANCELD)

 

#define STM32PERFORMANCE

 

#endif

 

 

to the definition of STM32PERFORMANCE!

So, returned to main.c,

#if (defined(STM32PERFORMANCE) && !defined(STM32F10X_MD))

 

#error ''Invalid configuration: MCU definition in Control stage parameters.h not compatible with selected board''

 

#endif

 

... and the Error-Message is given out.

What is to do?

- Change the Preprocessor-Defines?

- Change File Control stage parameters.h ?

Who has an idea, what is correct?

Thanks for answers

Martin

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gigi
ST Employee
Posted on September 18, 2012 at 17:52

Ciao Martin

I suppose that

#define STM32VALUEMD

 

shall be the corret value to be set in control stage.h.

You have a STM32100B-EVAL board that mounts a STM32F100 that is also called ''Value line''. You have already set the

STM32F10X_MD_VL

in your preprocessor define and the VL mean ''Value Line''.

So I think it can work.

Ciao

Gigi