cancel
Showing results for 
Search instead for 
Did you mean: 

Step response in STM32-Mckit

reman130488
Associate II
Posted on May 25, 2010 at 17:41

Step response in STM32-Mckit

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
bille.stello
Associate III
Posted on May 17, 2011 at 10:20

Hello,

you can adjust the increment of the target speed increment/decrement by manually editing the source file MC_Keys.c parameter SPEED_INC_DEC (line 57). Resoultion is 6 rpm so to set an increment of 500rpm you should write there 500/6 = 83.

Regards,

Billino