cancel
Showing results for 
Search instead for 
Did you mean: 

STEF48H28 Telemetry and status information

TIENHUA
Associate III

Hi Sir

I have a few technical questions regarding STEF48H28:

  1. Could you please clarify which specific telemetry and diagnostic data can be read digitally through the PMBus interface?

  2. Are the input voltage, output current, and internal temperature accessible as digital values via PMBus, or are these parameters only available in analog form through the IMON and TMON pins?

0 REPLIES 0