cancel
Showing results for 
Search instead for 
Did you mean: 

STBC08 charger state outputs, GPIO, pullups

Eliot Stock
Associate
Posted on October 09, 2017 at 18:36

Hi.

I have an STBC08 charger IC on a board here. It has two open drain output pins for state: CHARGE and POWER ON. It's this part:

http://www.st.com/content/st_com/en/products/power-management/battery-management-ics/battery-chargers/stbc08.html

 

The datasheet for the part has this to say about these two pins when they're in the '1' state:

'Output pin in high impedance (external pull-up needed).'

I have both these pins connected to a micro on which I've configured GPIO input pins with a pullup resistor. VDD on that micro is 3.0V. But when the pins go high on the STBC08, the micro does not see the input go high. The voltage on the output is about 1.2V, so, less than half of VDD for the micro. The micro is a Nordic Semiconductor nRF 52 series.

What could be the cause of this?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0