cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in LN298 and microcontroller

fatsi500
Associate
Posted on April 04, 2005 at 20:59

Problem in LN298 and microcontroller

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
fatsi500
Associate
Posted on May 17, 2011 at 10:18

hi,

i am trying to drive a dc motor (20v) using LN298 and ATMEL microcontroller, when i try to drive the dc motor with LN298 alone (without microcontroller) it works good.

and when i try the microcontroller alone it gives the right output (testing on leds)

but the problem apears when i try to connect the microcontroller directly to the LN298.

the LN298 takes its first state from the microcontroller and then the microcontroller stops (i doesnt respond to anything after that)

i tried to put ULN2003 between the microcontroller and LN298,

i also tried to put an inverter between them,

i also tried transistors and diodes but the same problem appears each time the microcontroller stops responding after it gives the first output to LN298

can any one help please...

onlyoneliveforever
Associate II
Posted on May 17, 2011 at 10:18

check your power supply

it seem that u don't have egnouh power

are using Batterys ??

the Vs = 20V MOTOR VOLTAGE

the VSS = 5V TTL/CMOS

[ This message was edited by: Cortex on 05-04-2005 00:30 ]