cancel
Showing results for 
Search instead for 
Did you mean: 

Need suggestion for Stepper/servo motor controller with encoder !!!!!

kishhor
Associate
Posted on January 16, 2009 at 08:37

Need suggestion for Stepper/servo motor controller with encoder !!!!!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
kishhor
Associate
Posted on May 17, 2011 at 10:15

Hi friends,

We are planning to shift from ''SILAB 8051 + Keil C51'' to ARM (cortex-M3),

for my new project 5-Axis CNC controller .

In that we have to generate pulses up to 2MHz & quadrature encoder for position sensing.

We have two options,

1. Luminary micro -> They have inbuilt dedicated motion control & quadrature encoder interface.

2. STM32 -> In STM32, which processor is suitable, Will I need some peripherals to implement above requirement ????????

Thanks in advance,

Kishor.

[ This message was edited by: kishhor on 17-01-2009 12:25 ]