cancel
Showing results for 
Search instead for 
Did you mean: 

L6205 , PWM

eyals111
Associate II
Posted on April 18, 2013 at 16:07

HI ,

1.can any one tell me how to PWM DC motor using L6205  ,via EN pin or

   INX pin  ?

2.how can i make the motor coasting (in PWM OFF)  ?

for the Table in the Datasheet 

when EN=1,     if IN1=0,IN2=1 => OUT1=GND  OUT2=VS

                       else IN1=1,IN2=0 = > OUT1=VS OUT=GND

how can i put the H bridge in HighZ (only 1 side ) ?

from what i understand PWM DC motor in specific direction there are 2 phase

PWM ON - the motor get  VS (Left H bridge side) and GND (High H bridge side)

PWM OFF - the motor is coasting (Left H bridge side is in High Z) and GND (High H bridge side)

 

#l6205 #dc-motor-control
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0