2020-06-17 3:27 AM
I am using Viper12A as aux supply for sensors in a bigger Power supply system for sensors. I need to know if the line rectification circuit is possible using Bridge rectifier network. The output power needed is less than 1W with 16V output.
Thanks in advance.
2020-06-17 8:01 AM
.
2020-06-17 8:01 AM
You will find such a rectifier if you have a look at the datasheet of the VIPER12A, pg. 7.
So, yes, of course you can.
BTW: the VIPERs always "see" DC voltage coming from the capacitor behind the rectifier. It doesn't care if it is rectified using a single rectifier, a bridge rectifier or a 3 phase rectifier.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.