2026-05-09 3:46 AM - last edited on 2026-05-09 9:47 AM by Peter BENSCH
Hello,
I am evaluating the VND5T100AJ-E for an automotive application where I need to drive a 24V contactor. My design requirement is i need to drive the IC through the PWM signal as input.
I have reviewed the datasheet but do not see explicit PWM frequency ratings. My concerns are:
Does the VND5T100AJ-E support continuous PWM switching for an inductive load?
If this device is not recommended for PWM, could you suggest a similar specification alternative part with the same specifications that is specifically designed for PWM input @stmicro
2026-05-09 10:00 AM
Welcome @Chiranjeevi9391, to the community!
TheVND5T100LAJ-E can also switch inductive loads, including via PWM. The switching frequency can be estimated based on the turn-on and turn-off delay times.
What PWM frequency are you planning to use?
Regards
/Peter
2026-05-09 10:45 AM