cancel
Showing results for 
Search instead for 
Did you mean: 

I am looking for a replacement of the Renesas driver HIP4086ABZ, 3-phase N-channel MOSFET drivers, specifically targeted for PWM motor control with a package size equal or lower. Thanks for your proposals

ALumb.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @ALumb.1​, to the community!

You could either look at the STDRIVE101 with max 75V bus voltage, alternatively the STDRIVE601 for 600V.

You can get more help from your local FAE or ST office.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.