cancel
Showing results for 
Search instead for 
Did you mean: 

How can we increase soft start time for VIPER319XDTR?

Kshah.21
Associate II

Dear sir,

We have followed STEVAL-VP319X1B development board schematic for converting 110V/230V AC to 5V DC. In one of board we found that inrush current limiting resistor is burn out. We have followed same part number for resistor which is in development kit BOM. Can you suggest how we can increase soft start time.

Thanks

Kadam

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14

Hi Peter Bensch,

If you used in any reference design, can provide suggestive PTC part number.

However with 10E 3W (R24), so far we haven't seen any burning issue.

Thanks

Kadam

If a PTC is an option, please contact PTC manufacturers as the correct part should be carefully selected.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter Bensch,

We are planning to use PTC : PTCEL17R600MBE.

Please share your thought for PTC.

I have attached datasheet for your reference.

Thanks

Kadam

Hi Peter Bensch,

PTC is quite costly as compare to inrush resistor (metal oxide, flame proof).

Currently we are using 10E, 5W resistor (ROX5SSJ10R).

I have attached datasheet for reference.

Do you feel tuning compensating network tuning can help us?

Thanks

Kadam

With this PCTEL there are probably only PTCEL17R600MBE or PTCEL13R600LBE in question, because the hold current is just sufficient, but you must then also take its losses into account.

On the other hand, a 5W resistor is of course also an option if its size is not a problem.

Tuning the compensation network unfortunately does not help at all with inrush current, but can improve the phase margin and other parameters depending on the input and output parameters.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.