cancel
Showing results for 
Search instead for 
Did you mean: 

EVAL-SCS001V1 USB Data lines

Circuit
Associate II

Hi

In this 

EVAL-SCS001V1 Board

I want to connect this board to my STM32F767ZI, BUT Data lines D+/D- on Its USB-C Connector are not connected to any test point. Is there any workaround this? I can solder wires to for example A side of this connector(D+/D-) but then B side will be left unconnected. I can live with the fact that USB CABLE will work in only 1 orientation when inserted in USB-C Receptable but i am unsure of any other consequences that it will cause? Power delivery contracts/CC1/2, etc.. 

I know ST offers another Development board STEVAL-ISC005V1 where these signals are available but don't need so many Voltage Outputs and EVAL-SCS001V1 fits perfectly.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

On the EVAL‑SCS001V1 the USB‑C connector is intended only for power‑delivery, not as a USB data port, which is why D+/D- are not brought out. In principle you can solder to one side’s D+/D- pads and accept that the plug will only work in one orientation; the CC pins handled by the STM32G0 on the board will still negotiate the PD contract, and leaving the other D+/D- pair unconnected does not affect PD itself.

However:

  • You would need very short, well‑routed wires to have any chance of reliable USB signalling
  • The board was not designed or EMC‑qualified for this use, so ST cannot guarantee signal integrity or compliance
  • For a supported USB connection, STEVAL‑ISC005V1 (or a separate USB connector on your STM32F767ZI board) is indeed the recommended tool

So: your workaround may function for lab experiments, but it is a hack and not recommended for a final design.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

On the EVAL‑SCS001V1 the USB‑C connector is intended only for power‑delivery, not as a USB data port, which is why D+/D- are not brought out. In principle you can solder to one side’s D+/D- pads and accept that the plug will only work in one orientation; the CC pins handled by the STM32G0 on the board will still negotiate the PD contract, and leaving the other D+/D- pair unconnected does not affect PD itself.

However:

  • You would need very short, well‑routed wires to have any chance of reliable USB signalling
  • The board was not designed or EMC‑qualified for this use, so ST cannot guarantee signal integrity or compliance
  • For a supported USB connection, STEVAL‑ISC005V1 (or a separate USB connector on your STM32F767ZI board) is indeed the recommended tool

So: your workaround may function for lab experiments, but it is a hack and not recommended for a final design.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.