cancel
Showing results for 
Search instead for 
Did you mean: 

Writing to EEPROM of STM32L051K8?

okals.1492
Associate

I am trying to flash a data to `EEPROM` of `STM32L051K8` with HAL library. This functions keeps returning `HAL_ERROR`. With debug i found the problem. 

In HAL Flash library before writing data to `EEPROM` it checks for error flags with `FLASH_WaitForLastOperation` and `FLASH_FLAG_WRPERR`(write protection error flag) is set. So it returns `HAL_ERROR` but `HAL_FLASHEx_DATAEEPROM_Unlock` returns `HAL_OK`.

HAL_StatusTypeDef setCommAddressState(void){
    	HAL_StatusTypeDef status;
    	status = HAL_FLASHEx_DATAEEPROM_Unlock();
    	if (status != HAL_ERROR)
    	{
    		status = HAL_FLASHEx_DATAEEPROM_Program(FLASH_TYPEPROGRAMDATA_BYTE, COM_ADDRESS_STATE_ADDRESS, comAddressStateData);
    		if (status == HAL_OK){
    			comAddressState = comAddressStateData;
    		}
    	}
    	HAL_FLASHEx_DATAEEPROM_Lock();
    	return status;
    }

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ty.locke
Associate II

I haven't had any issues writing to flash with the HAL library on the STM32L072. Have you tried erasing your address range before attempting to write?

okals.1492
Associate

Yes i did and it didnt work. I tried a do while loop and it is ok now. after trying several time error flag did not set but i feel like there is an other problem and i am not sure.