2018-11-18 10:16 PM
I'm trying to build an example project for the STSPIN32F0A in TrueStudio but I'm getting a few errors. I was hoping someone here might be able to help me. I picked out the STEVAL-SPIN3202 - BullRunning project and didn't make any changes. It seemed to save this project in my 'Users' folder and not my Workspace. I then opened the project in TrueStudio using File > Open projects from file system and then pointed it to the folder under C:\Users\,username.
Once I could see it in my list in TS, I then rebuilt the index and then refreshed all files. I then tried building the project and here are the errors that I see:
region `RAM' overflowed by 240 bytes STEVAL-SPIN3202 - BullRunning C/C++ Problem
STEVAL-SPIN3202 - BullRunning.elf section `._user_heap_stack' will not fit in region `RAM' STEVAL-SPIN3202 - BullRunning C/C++ Problem
'OverVoltageFlag' may be used uninitialized in this function [-Wmaybe-uninitialized] mc_tasks.c /STEVAL-SPIN3202 - BullRunning/Application/User line 814 C/C++ ProblemThe last one is a warning. I'm guessing the error is an RAM overflow error but I have no idea how to fix it so any help would be appreciated. Also, is this the right process to open a Motor Workbench Project into TrueStudio?
2018-11-27 1:28 AM
Hello Hrishikesh B,
Did you see the following limitation in the Release note?:
I hope it can help you,
Thanks and best regards,
Claire
2018-11-27 2:02 AM
Hello Claire,
Thanks. Could you please point me to these release notes? Also, is this fixed in STM32CUbeMX 5?
I've changed it to "Optimize for Speed (-Ofast)", however, I'm still seeing the same error. Please see the attached screenshot. I tried "OPtimize for size (-Os)" and that too shows the error.
Best
Hrishikesh
2018-11-27 7:33 AM
Hello Hrishikesh B,
I was referring of the x-cube-mcsdk version 5.2 release note that you can find here:
The release note is accessible directly from the MC workbench if you click on documentation field.
After discussing with the team, we found out that there is a known problem with Atollic TrueSTUDIO and STM32F0. It will be corrected with next MCSDK release arriving in few weeks and working with STM32CubeMx 5.
Best regards,
Claire
2018-11-27 8:22 AM
I see. Let me try SW4STM32. Any particular IDE you would recommend for this particular SDK?
Best
Hrishikesh
2018-11-27 8:33 AM
Keil has a free license for ST CM0(+) parts, that's likely to be better supported and less amateurish that some of the alternatives, especially when fighting issues specific to GNU/GCC and Eclipse based stuff.
2018-11-27 9:26 AM
I agree with Clive Two.Zero. Keil or IAR are more safe IDE (and with different compiler). Please check in the release note with which version the MCSDK has been tested.
Claire
2018-11-29 6:35 AM
Thank you, that helped.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.